Update HSC application data

High-speed counter (HSC) configuration is defined in the HSC application data, and is usually only configured once before programming the HSC instruction. Changes made to the HSC application data (HSCAppData parameter) are ignored while the HSC is counting.
To update HSC application data
  1. Update HSCAppData.
  2. Call the HSC instruction with command 0x03 (set/reload).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal