Configure a high-speed counter (HSC) user interrupt

A user interrupt causes the controller to suspend the task it is performing, perform a different task, and then return to the suspended task at the point where the task was suspended.
Micro850
L50E and
Micro870
L70E controllers support up to six HSC user interrupts that can be used to execute selected user logic at a pre-configured event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal