ROL (rotate left)
The ROL instruction rotates the DINT type input by NbR bits to the left in a circular form and fills the bits on the right with the bits that are rotated.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.ROL

ROL

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
|
IN | Input | DINT | Integer value. |
NbR | Input | DINT | Number of 1-bit rotations (in set [1..31]). |
ROL | Output | DINT | Left rotated value. When NbR <= 0, no change occurs. |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. |
ROL examples
ROL function block diagram example

ROL ladder diagram example

ROL structured text example

(* ST Equivalence: *) result := ROL (register, 1); (* register = 2#0100_1101_0011_0101*) (* result = 2#1001_1010_0110_1010*)
Results

Provide Feedback