LFL (LIFO load)

The LFL instruction is used to load the data (8 bit, 16 bit, 32 bit and 64 bit) into a user-created one-dimensional array called LIFO stack. LFL and LFU instructions are used in pairs.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
LFL
LFL
LFL parameters
Parameter
Parameter Type
Data Type
Description
Execute
Input
BOOL
Instruction block enable.
  • TRUE: If rising edge is detected, start the LFL operation.
  • FALSE: Rising edge is not detected.
Src
Input
ANY_ELEMENTARY
The Src operand is the address of the value to fill the current available position sin the LIFO stack.
Element data types supported:
  • DWORD, REAL, TIME, DWORD, REAL, TIME, DATE, LWORD, ULINT, LINT, LREAL, BOOL, SINT, USINT, BYTE, INT, UINT, WORD, DINT, UDINT.
  • Variables and one-dimensional arrays such as Array [1] or Array[Index].
  • String is not supported.
LIFO
Input
ANY_ELEMENTARY
The starting address of the stack. LIFO must be configured the same for the LFL and LFU instructions.
Element data types supported:
  • DWORD, REAL, TIME, DWORD, REAL, TIME, DATE, LWORD, ULINT, LINT, LREAL, BOOL, SINT, USINT, BYTE, INT, UINT, WORD, DINT, UDINT.
  • Only one dimension is supported.
  • String is not supported.
LIFOCon
Input
FF_LF_CON
LIFO configuration and control. The same configuration must be configured for LFL and LFU instructions. Use the FF_LF_CON data type to configure Position and Length.
Full
Output
BOOL
Indicates when the LIFO stack is full.
  • TRUE: When Length is equal to Position.
  • FALSE: When Position is greater than or equal to zero and less than Length.
Empty
Output
BOOL
Indicates when the LIFO stack is empty.
  • TRUE: When Position equals zero.
  • FALSE: When Position is not equal to zero.
Error
Output
BOOL
Indicate the existence of an error condition.
  • TRUE: Operation encountered an error.
  • FALSE: Operation completed successfully or the instruction is not executing.
ErrorID
Output
USINT
A unique numeric that identifies the error. The errors are defined in the LFL error codes.
Done
Output
BOOL
Indicate when operation is completed.
  • TRUE: Operation completed successfully.
  • FALSE: Operation encountered an error condition or the LFL instruction is not executing.
LFL and LFU error codes
Error code
Error description
0
No error.
1
LFL Src data type is not supported.
2
LFU Dest data type is not supported.
3
LIFO data type is not supported.
4
Src and Dest data type mismatch with the LIFO data type.
Corrective action:
LFL Src parameter and LFU Dest parameter data type should match with the LIFO array data type.
5
LIFO: Array dimension is not supported.
Corrective action:
LIFO only supports one-dimensional arrays.
6
LIFOCon control Length exceeds LIFO array size.
Corrective action:
LIFOCon control Length cannot exceed the LIFO array size.
7
LIFOCon Length exceeds the max length.
8
LIFOCon Length is zero.
9
LIFOCon Position exceeds the LIFOCon Length.
10
LFL control Length and Position are equal.
11
LFU control Position is zero.
12
LFL or LFU array dimension is not supported.
Corrective action:
LFL and LFU only support one-dimensional arrays.
13
LFL or LFU DestOffset exceeds Dest array size.

LFL examples

LFL function block diagram example
LFL function block diagram example
LFL ladder diagram example
LFL ladder diagram example
LFL structured text example
LFL structured text example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal