AVE (average)

The AVE instruction calculates a running average over a number of defined samples and stores the value at each cycle.
Operation details:
  • The defined number of samples (N) cannot exceed 127.
  • When setting or changing the value for N, set RUN to FALSE, then set it back to TRUE.
  • If the RUN command is FALSE (reset mode), the output value is equal to the input value.
  • When the maximum number of stored values is reached, the first stored value is erased by the last one.
  • Using floating-point data types could result in inaccurate calculations due to the rounding limitations inherent in floating-point mathematics.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
AVE
AVE
AVE parameters
Parameter
Parameter Type
Data Type
Description
RUN
Input
BOOL
  • TRUE = run
  • FALSE = reset
XIN
Input
REAL
Any real variable.
N
Input
DINT
Application defined number of samples.
XOUT
Output
REAL
Running average of XIN value.
ENO
Output
BOOL
Enables output. Applies to ladder diagram programs.

AVE examples

AVE function block diagram example
AVE function block diagram example
AVE ladder diagram example
AVE ladder diagram example
AVE structured text example
AVE structured text example
(* ST Equivalence: AVE1 an instance of an AVE block *) AVE1((auto_mode & store_cmd), sensor_value, 100); ave_value := AVE1.XOUT;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal