ANY_TO_WORD
The ANY_TO_WORD instruction converts a value to a 16-bit Word value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10, Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.ANY_TO_WORD

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
| |
i1 | Input | BOOL SINT USINT BYTE INT DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME DATE STRING | Any value other than a Word value. |
o1 | Output | WORD | A Word value. | |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. | |
ANY_TO_WORD structured text example
bres := ANY_TO_WORD (true); | (* bres is 1 *) |
tres := ANY_TO_WORD (t#0s46ms); | (* tres is 46 *) |
mres := ANY_TO_WORD ('0198'); | (* mres is 198 *) |
Provide Feedback