ANY_TO_UINT

The ANY_TO_UINT instruction converts a value to an Unsigned Integer value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
ANY_TO_UINT
ANY_TO_UINT
ANY_TO_UINT parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
When set to true, the instruction is enabled.
  • TRUE: Execute the current computation.
  • FALSE: There is no computation.
Applies to ladder diagram programs.
i1
Input
BOOL
SINT
USINT
BYTE
INT
WORD
DINT
UDINT
DWORD
LINT
ULINT
LWORD
REAL
LREAL
TIME
DATE
STRING
Any non-Unsigned Integer value.
o1
Output
UINT
An Unsigned Integer value.
ENO
Output
BOOL
Enables output. Applies to ladder diagram programs.

ANY_TO_UINT structured text example

(* ST Equivalence: *)
bres := ANY_TO_UINT (true);
(* bres is 1 *)
tres := ANY_TO_UINT (t#0s46ms);
(* tres is 46 *)
mres := ANY_TO_UINT ('0198');
(* mres is 198 *)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal