ANY_TO_UDINT

The ANY_TO_UDINT instruction converts a value to a 32-bit Unsigned Double Integer value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
ANY_TO_UDINT
ANY_TO_UDINT
ANY_TO_UDINT parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
When set to true, the instruction is enabled.
  • TRUE: Execute the current computation.
  • FALSE: There is no computation.
Applies to ladder diagram programs.
i1
Input
BOOL
SINT
USINT
BYTE
INT
UINT
WORD
DINT
DWORD
LINT
ULINT
LWORD
REAL
LREAL
TIME
DATE
STRING
Any value other than an Unsigned Double Integer.
o1
Output
UDINT
A 32-bit Unsigned Double Integer value.
ENO
Output
BOOL
Enables output. Applies to ladder diagram programs.

ANY_TO_UDINT structured text example

(* ST Equivalence: *)
bres := ANY_TO_UDINT (true);
(* bres is 1 *)
tres := ANY_TO_UDINT (t#1s46ms);
(* tres is 1046 *)
mres := ANY_TO_UDINT ('0198');
(* mres is 198 *)

Instruction behavior changes starting from firmware revision 23.012

When converting REAL or LREAL values to the UDINT data type, the following rules apply:
  • Positive values
    • Values from 0 through 2³¹ − 1 can be converted to the UDINT data type.
    • Values exceeding 2³¹ − 1 are clamped to 2³¹ − 1.
  • Negative values
    • Values from −1 through −2³¹ can be converted to the UDINT data type.
    • Values smaller than −2³¹ are clamped to 2³¹.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal