ANY_TO_TIME

The ANY_TO_TIME instruction converts a non-Time or non-Date value to a Time value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
ANY_TO_TIME
ANY_TO_TIME
ANY_TO_TIME parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
When set to true, the instruction is enabled.
  • TRUE: Execute the current computation.
  • FALSE: There is no computation.
Applies to ladder diagram programs.
i1
Input
BOOL
SINT
USINT
BYTE
INT
UINT
WORD
DINT
UDINT
DWORD
LINT
ULINT
LWORD
REAL
LREAL
STRING
Any positive value other than a Time or Date data type.
IN (or integer part of IN if it is real) is the number of milliseconds.
STRING (number of milliseconds, for example, a value of 300032 represents 5 minutes and 32 milliseconds).
o1
Output
TIME
Time value represented by IN. A value of 1193h2m47s295ms indicates an invalid time.
ENO
Output
BOOL
Enables output. Applies to ladder diagram programs.

ANY_TO_TIME structured text example

(* ST Equivalence: *)
ares := ANY_TO_TIME (1256);
(* ares := t#1s256ms *)
rres := ANY_TO_TIME (1256.3);
(* rres := t#1s256ms *)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal