ANY_TO_LREAL

The ANY_TO_LREAL instruction converts any value to a Long Real value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
ANY_TO_LREAL
ANY_TO_LREAL
ANY_TO_LREAL parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
When set to true, the instruction is enabled.
  • TRUE: Execute the current computation.
  • FALSE: There is no computation.
Applies to ladder diagram programs.
i1
Input
BOOL
SINT
USINT
BYTE
INT
UINT
WORD
DINT
UDINT
DWORD
LINT
ULINT
LWORD
REAL
TIME
DATE
STRING
Any value other than a Long Real.
o1
Output
LREAL
A Long Real value.
ENO
Output
BOOL
Enables output. Applies to ladder diagram programs.

ANY_TO_LREAL structured text example

(* ST Equivalence: *)
bres := ANY_TO_LREAL (true);
(* bres is 1.0 *)
tres := ANY_TO_LREAL (t#1s46ms);
(* tres is 1046.0 *)
ares := ANY_TO_LREAL (198);
(* ares is 198.0 *)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal