ANY_TO_DINT

The ANY_TO_DINT instruction converts a value to a 32-bit Double Integer value.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
LC10,
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers.
ANY_TO_DINT
ANY_TO_DINT
ANY_TO_DINT parameters
Parameter
Parameter Type
Data Type
Description
EN
Input
BOOL
Instruction enable.
  • TRUE: Execute the conversion to the 32-bit Double Integer computation.
  • FALSE: There is no computation.
Applies only to ladder diagram programs.
i1
Input
BOOL
SINT
USINT
BYTE
INT
UINT
WORD
UDINT
DWORD
LINT
ULINT
LWORD
REAL
LREAL
TIME
DATE
STRING
Any value other than a Double Integer.
o1
Output
DINT
A 32-bit Double Integer value.
ENO
Output
BOOL
Enable output.
Applies only to ladder diagram programs.

ANY_TO_DINT structured text example

(* ST Equivalence: *)
bres := ANY_TO_DINT (true);
(* bres is 1 *)
tres := ANY_TO_DINT (t#1s46ms);
(* tres is 1046 *)
mres := ANY_TO_DINT ('0198');
(* mres is 198 *)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal