Timer instruction configuration

Time accuracy refers to the time between the moment the processor enables a timer instruction and the moment the processor completes the timed interval.
The processor uses the following information from the timer instruction:
  • Timer
    : The timer control address in the timer area of data storage.
  • Time Base
    : Determines how the timer operates.
  • Preset
    : Specifies the value that the timer must reach before the processor sets the done bit.
  • Accumulated value
    : The number of time increments the instruction has counted. When enabled, the timer updates this value continually.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal