Examine If Closed (XIC)

XIC supports a Boolean operation between a connection line state and a Boolean variable.
XIC
The state of the connection line on the right of the contact is the logical AND between the state of the left connection line and the value of the variable associated with the contact.
XIC example
XIC example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal