Output Latch (OTL)

OTL enables a Boolean output of a connection line Boolean state.
OTL
OTL
The associated variable is set to TRUE when the Boolean state of the left connection becomes TRUE. The output variable keeps this value until an inverse order is made by an OTU. The state of the left connection is propagated into the right connection. The right connection must be connected to the right vertical power rail, unless you have parallel coils, where only the upper coil must be connected to the right vertical power rail.
The associated Boolean variable must be an output or be user-defined.
OTL example
OTL example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal