Output Energize (OTE)

OTE supports a Boolean output of a connection line Boolean state.
OTE
LD - OTE
The associated variable is assigned with the Boolean state of the left connection. The state of the left connection is propagated into the right connection. The right connection must be connected to the right vertical power rail, unless you have parallel coils, where only the upper coil must be connected to the right vertical power rail.
The associated Boolean variable must be an output or be user-defined.
OTE example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal