ARL (ASCII read line)
The ARL instruction reads a line of ASCII characters from the buffer, up to and including the termination characters, and stores them in a string.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro820
L20E, Micro850
L50E, and Micro870
L70E controllers.ARL

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
IN | Input | BOOL | Rung input state.
|
ARLInput | Input | Read a line of ASCII characters from the buffer. The maximum is 82. Use the ARDARL data type to define the Channel, Length, and Cancel parameters for the ARDLInput. | |
Q | Output | BOOL | Indicates when the read line from the input buffer is ongoing or complete. Outputs of this instruction are updated asynchronously from the program scan. Output Q cannot be used to re-trigger the instruction because IN is edge triggered.
|
Destination | Output | ASCIILOCADDR | The string element where the characters are stored. |
NumChar | Output | UINT | The number of characters in the line, including the termination character. |
Error | Output | BOOL | Indicates the existence of an error condition.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in ABL error codes. |
Error code | Error description |
|---|---|
03 | Transmission cannot be completed because the Clear-to-Send signal was lost. |
06 | Illegal parameter was detected. |
07 | Cannot complete ASCII send or receive because channel configuration has been shut down using the channel configuration dialog. |
08 | Cannot complete ASCII Write due to an ASCII transmission already in progress. |
09 | ASCII communication requested is not supported by current channel configuration. |
10 | The Cancel was set, stopping instruction execution. No action required. |
11 | The requested length for the string is either invalid, a negative number, greater than 82, or 0. Applies to ARD and ARL function blocks. |
14 | The ACL function block was canceled. |
16 | Serial port is not supporting RTS or CTS control lines. |
ARL examples
ARL function block diagram example

ARL ladder diagram example

ARL structured text example

Provide Feedback