Math instructions

Use the Math instructions to perform mathematical calculations.
Arithmetic instructions
Function
Description
Returns the absolute value of a Real value.
Adds two or more Integer, Real, Time, or String values.
Divides two Integer or Real values.
Performs a Modulo calculation on Integer values.
Multiplies two or more Integer or Real values.
Converts a value to a negative.
Subtracts one Integer, Real, or Time value from another Integer, Real, or Time value.
Truncates Real values, leaving just the Integer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal