USB port configuration page

Use the USB Port configuration page to do the following actions:
  • Turn on or turn off the USB port.
  • View the basic USB port settings.
USB port configuration page settings
Setting
Description
Status
Turns on or turns off the USB port. The USB port is turned on by default.
Suspend state
Shows the suspended state of the USB port. The USB port is not suspended by default.
Bus speed
Shows the highest supported USB bus speed. Options are:
  • High speed
  • Full speed
  • Low speed
Full speed
is the default setting.
Mode
Shows the current mode of the USB port. Options are:
  • Slave mode
  • Host mode
Slave mode
is the default setting.
State
Shows the state of the USB port. Options are:
  • Initializing.
  • Fault Initialized.
  • Configured.
  • Ready.
Ready
is the default setting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal