Select remote LCD variables to monitor

Use the
LCD variables
view to select the variables you want to monitor using the remote LCD.
Prerequisites
  • The controller is offline.
  • Download the project and project values to the controller.
To select LCD variables to monitor
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Remote LCD
    .
  3. On the
    Remote LCD
    configuration page, select
    LCD variables
    .
  4. In
    LCD variables
    , select the
    LCD display
    checkbox of the variables you want to monitor.
  5. Verify that
    Communication
    is not set to
    No access
    for the variables that you want to monitor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal