Import recipes

Use the
Recipe
configuration page to import recipes from an M8A file on your computer. You can import up to 10 recipes to the controller.
The imported recipes overwrite all the recipes in the controller if any.
Prerequisites
  • The controller is offline.
  • Have an M8A file of recipes.
To import recipes
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Recipe
    .
  3. On the
    Recipe
    configuration page, select
    Import
    .
  4. In
    Import recipe
    , select
    Browse
    .
  5. In
    Open
    , locate and select the M8A file you want to import, and then select
    Open
    .
  6. In
    Import recipe
    , select
    Import
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal