Export recipes

Use the
Recipe
configuration page to export recipes to your computer. By default, recipes are exported as an M8A file to the Downloads folder. When a file with the same name exists, a number will be appended to the exported file.
Prerequisites
  • One or more recipes are added.
To export recipes
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Recipe
    .
  3. On the
    Recipe
    configuration page, select
    Export
    .
  4. (optional) In
    Export recipe configurations
    , select the export path and enter the file name as needed.
  5. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal