Download recipes

Use the
<controller-name>: Manage recipes
page to download recipes to the memory card to update the recipes for the controller project.
Prerequisites
  • The controller is online.
To download recipes
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Recipe
    .
  3. On the
    Recipe
    configuration page, select
    Manage recipes
    .
  4. In
    <controller-name>: Manage recipes
    , select Download recipe icon.
  5. In
    Download recipes to memory card
    , select
    Browse
    .
  6. In
    Select folder
    , find and select the recipe file, and then select
    OK
    .
  7. In
    Download recipes to memory card
    , select
    Download
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal