Delete recipe files from the controller

Delete the recipe files from the memory card when the recipes are no longer part of the current controller project.
Prerequisites
  • The project is online.
  • One or more recipes are added.
To delete a recipe set from the controller
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Recipe
    .
  3. On the
    Recipe
    configuration page, select
    Manage recipes
    .
  4. In
    <controller-name>: Manage recipes
    , select Delete recipe button.
  5. In
    Delete recipes from memory card
    , select the recipe files you want to delete, and then select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal