Add variables to a recipe

Recipe files save custom lists of data associated with a recipe. Consider the following requirements when adding variables to a recipe:
  • Recipe variables can be of simple data types.
  • Recipe variables can contain array elements with simple data types and with up to three dimensions.
  • Recipe variables must be Read/Write.
  • A recipe supports up to four string variables.
  • A string variable can contain up to 252 characters.
Prerequisites
  • The project is offline.
To add variables to a recipe
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Recipe
    .
  3. On the
    Recipe
    configuration page, from the
    Recipe
    list, select the added recipe to which you want to add variables.
  4. Double-click
    Select variables
    or select Browse button to open the variable selector.
  5. In the variable selector, select the variable, and then select
    Select
    .
    TIP: To change the order of the added recipe variables, drag the row headers of the variables to the desired place.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal