Rename an FBAxis

After adding a 2080-MOT-HSC plug-in module and activating it with
Feedback Axis
:
  • On the
    2080-MOT-HSC
    configuration page, a
    Feedback Axis
    node is created. Select the node to view and configure the settings on the following pages:
  • On the PTO Motion configuration page, a
    FBAxis<x>
    checkbox is added. The checkbox is selected and read-only by default.
To rename an FBAxis
  1. In
    Project Organizer
    , go to
    I/O Configurations
    Plug-in
    , and then double-click
    2080-MOT-HSC
    .
  2. On the
    2080-MOT-HSC
    page, select
    Feedback Axis
    .
  3. On the
    FBAxis<x> - General
    configuration page, in the
    Axis name
    box, enter the new name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal