Add variables to a data set

Data logs contain data sets and record the data values of a defined set of variables that you added to the controller project. Use the
Data Log
configuration page to add variables to a data set.
Prerequisites
  • The controller is offline.
To add variables to a data set
  1. In
    Project Organizer
    , double-click the controller to open the controller application workspace.
  2. In the
    Controller
    tree, select
    Data log
    .
  3. On the
    Data Log
    configuration page, select an added data set to which you want to add the variables.
  4. Double-click
    Select variable
    or select Browse button to open the variable selector.
  5. In the variable selector, select the variable, and then select
    Select
    .
    TIP: To change the order of data set variables, drag the row headers of the variables to the desired place.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal