Memory allocation

The following section introduces the
Micro800
controller memory in
FactoryTalk Design Workbench
with examples.
  • For data files, a word is the equivalent of 16 bits of memory.
  • For program files, a word is the equivalent of a ladder instruction with one operand.
Data file examples
Data File
Equals
One integer data file element
One user word
One long word file element
Two user words
One timer data file element
Three user words
Program file examples
Program File
Consumes
Each XIC instruction with one operand
One user word
Each EQU instruction with two operands
Two user words
Each ADD instruction with three operands
Three user words
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal