View the controller mode

When connected to a
Micro800
controller, use
Connection
to view the controller mode.
Prerequisites
  • The controller is online.
To view the controller mode
  • In
    Connection
    , select  open dropdown list rectangle to expand the controller information. Available controller modes are as follows:
    • Program
      : The controller is in the non-running mode and can be programmed. The mode cannot be changed remotely.
    • Remote program
      : The controller is in the non-running mode and can be programmed. The mode can be changed remotely.
    • Run
      : The controller is in the running mode. The mode cannot be changed remotely.
    • Remote run
      : The controller is in the remote running mode, displaying the connected values from the controller in
      FactoryTalk Design Workbench
      . The mode can be changed remotely.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal