View the controller fault status

When connected to the
Micro800
controller, use
Connection
to view the controller fault status.
Prerequisites
  • The controller is online.
To view the controller fault status
  1. (optional) If
    Connection
    is hidden, open it by doing one of the following:
    • From the
      View
      menu, select
      Connection
      .
    • Select Online center button to open the
      Online center
      .
  2. In
    Connection
    , beside the controller name and catalog number, check the color of the toggle. If a fault occurs, the toggle turns red with an error icon.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal