Configurations on the controller diagnostics page

Configurations on the controller diagnostics page
Configuration
Description
Controller Identity
Displays the catalog number, firmware revision, series, serial number, and firmware boot code of the controller.
Startup
Mode Behavior
Controls how the controller behaves during power-up.
Fault Override
Displays the clear fault option during power-up.
Memory Module or Memory Card
Load on power up
Determines if the controller restores the project from the memory module at power-up. The setting is selected in the memory module at power-up.
Overwrite Ethernet settings
Determines if the current Ethernet settings will be overwritten by the settings in the memory module when restoring from the memory module.
This setting only resides in the controller project and is not part of the memory module settings.
Unlike load-always project settings that are backed up to and then read at power-up from the memory card,
Overwrite Ethernet settings
are read at power-up from the project setting residing in the controller and cannot be read directly from the memory card.
Include variable values upon backup or restore
Determines whether to include the controller values when backing up or restoring the controller project.
Catalog ID
Displays the model number of the controller or memory module.
Project version
Displays the version of the project in the controller or memory module.
Controller Information
CPU up time
Displays the total duration that the CPU has been active since its most recent power-up.
Communication utilization
Displays the communication buffer space utilization rate of the current system.
Summary
Displays:
  • Whether the project in the memory module is compatible with the controller and controller firmware.
  • Whether the password in the memory module matches the password in the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal