User-programmed socket statistics for Micro820 L20E, Micro850 L50E, and Micro870 L70E controllers

The user-programmed socket protocol monitors socket statistics for
Micro820
L20E,
Micro850
L50E, and
Micro870
L70E controllers. In
FactoryTalk Design Workbench
, use socket instructions in controller programs to create and open sockets for communications using Transmission Control Protocol (TCP) and User Datagram Protocol (UDP).
Socket instruction blocks include:
The parameters in the following table are available when you select
User-programmed sockets
from the
Protocols
list.
Ethernet communication statistics monitoring in real time
Parameter
Description
Total available
Displays the maximum number of supported socket instances.
Created
Displays the number of created socket instances.
For more information, see the SOCKET_CREATE instruction.
TCP connections
Displays the number of TCP instances.
Clients
Displays the number of socket instances opened as TCP clients.
Servers
Displays the number of socket instances opened as TCP servers.
Non-configured
Displays the number of socket instances that are not configured yet.
UDP datagrams
Displays the number of socket instances opened as UDP.
Packets
TCP success - Read
Displays the number of read TCP packets.
TCP success - Write
Displays the number of written TCP packets.
TCP failure - Read
Displays the number of unread TCP packets.
For more information, see the SOCKET_READ instruction block.
TCP failure - Write
Displays the number of unwritten TCP packets.
For more information, see the SOCKET_WRITE instruction block.
UDP success - Read
Displays the number of read UDP packets.
UDP success - Write
Displays the number of written UDP packets.
UDP failure - Read
Displays the number of unread UDP packets.
For more information, see the SOCKET_READ instruction block.
UDP failure - Write
Displays the number of unsent UDP packets.
For more information, see the SOCKET_WRITE instruction block.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal