EtherNet/IP overview statistics for Micro850 L50E and Micro870 L70E controllers

The EtherNet/IP overview protocol monitors Ethernet statistics for
Micro850
L50E and
Micro870
L70E controllers.
Statistics monitored and displayed in real time
Field
Description
TCP Connections
Active TCP connections
Displays the current number of active TCP connections for EtherNet/IP messaging.
Maximum TCP connections
Displays the maximum number of TCP connections supported for EtherNet/IP messaging.
Unconnected
Sent packets per second
Displays the number of EtherNet/IP unconnected messages or packets sent in the last second. By default, the number increments by one approximately every two seconds because of a task that checks the controller's connection status.
Received packets per second
Displays the number of EtherNet/IP unconnected messages or packets received in the last second. By default, the number increments by one approximately every two seconds because of a task that checks the controller's connection status.
Total packets sent
Displays the cumulative number of EtherNet/IP unconnected messages or packets sent.
Total packets received
Displays the cumulative number of EtherNet/IP unconnected messages or packets received.
Connected
Sent packets per second
Displays the number of EtherNet/IP connected messages or packets sent in the last one second.
Received packets per second
Displays the number of EtherNet/IP connected messages or packets received in the last one second.
Total packets sent
Displays the cumulative number of EtherNet/IP connected messages or packets sent.
Total packets received
Displays the cumulative number of EtherNet/IP connected messages or packets received.
I/O Packets Per Second
I/O packets per second sent (actual)
Displays the number of Class 1 EtherNet/IP packets the system transmitted in the last one second.
I/O packets per second received (actual)
Displays the number of Class 1 EtherNet/IP packets the system received in the last one second.
I/O packets per second total (actual)
Displays the total number of Class 1 EtherNet/IP packets the system received, sent, inhibited, and rejected in the last one second.
I/O packets per second rejected (actual)
Displays the number of Class 1 EtherNet/IP packets the system rejected in the last one second.
I/O Packets Counts
I/O packets sent
Displays the cumulative number of Class 1 EtherNet/IP packets the system transmitted.
I/O packets received
Displays the cumulative number of Class 1 EtherNet/IP packets the system received.
I/O packets rejected
Displays the cumulative number of Class 1 EtherNet/IP packets the system rejected.
These packets were messages received, and then rejected, because the connection was closed or there was a duplicate multicast address.
I/O packets missed
Displays the cumulative number of Class 1 EtherNet/IP packets that were not received in order.
Each UDP packet has a sequence number and if a packet is missing (corrupted or dropped), the system will recognize this void upon receipt of the next packet received. Missed counter increments by the number of packets missed.
I/O packets total
Displays the total number of Class 1 EtherNet/IP packets the system received, sent, inhibited, and rejected.
Application Connections
Type
Displays the Class of the connection: Class 1 or Class 3.
Status
Displays the state of the connection: Active and Inactive.
Uptime
Displays the elapsed time for the connection that has been maintained.
Serial Number
Displays the unique identifier for each connection.
O->T Packet Size
Displays the size of Originator to Target Packet Data in bytes.
T->O Packets Size
Displays the size of Target to Originator Packet Data in bytes.
Missed Packet Rx
Displays the number of packets that are lost because of that particular connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal