Add variables for data protection
Use
Data protection
to select multiple user-defined global variables that retain their values when:- Restoring a controller project from a memory module (available forMicro820L20E,Micro850L50E, andMicro870L70E controllers).
- Downloading a project, programs, variables, and controller configurations to aMicro800controller (available forMicro820L20E,Micro850L50E, andMicro870L70E controllers).
Data protection supports up to 60 user-defined variables of the following types:
- Simple data types, excluding STRING
- Arrays with up to three dimensions
To add variables for data protection
- OpenData protectionby doing one of the following:
- InProject Organizer, right-click the controller, and then selectData Protection.
- InProject Organizer, select the controller, and then from the menu bar, select .
- InData protection, double-clickSelect variableor select
. - In the variable selector, find and select the variable, and then selectSelect.
- InData protection, selectOK.To delete a variable fromData protection, right-click the variable, and then selectDelete.
Provide Feedback