Run mode change actions

The following table explains the supported and unsupported changes during run mode change (RMC).
Run mode change actions
Category
Supported Action
Unsupported Action
Configuration
  • Manage data logs and recipes.
  • Export data logs, recipes, DNP3 mappings, Modbus mappings, and PCCC mappings.
Change, add, or delete controller or I/O configurations.
Variables and data types
  • Create global variables and change their attributes.
  • Change the following attributes of global variables that are added before entering RMC:
    • Comments
    • Alias
    • Retained
  • Change or remove local variables that are not referenced by
    Micro800
    controller configuration.
  • Delete or change the following attributes of local variables that are referenced by
    Micro800
    controller configuration:
    • Comments
    • Alias
    • Retained
  • Create, change or remove defined words.
  • Export global and local variables.
  • Delete or change the attributes of local variables that are referenced by
    Micro800
    controller configuration, excluding
    Comments
    ,
    Alias
    , and
    Retained
    .
  • Delete existing global variables.
  • Change variable attributes or add or delete variables in a user-defined function block (UDFB) that is referenced by a global variable.
  • Create, remove, or change the attributes of user-defined arrays and structures, excluding
    Comments
    .
  • Change or remove the project value of variables.
  • Change the data type of dimensional variables.
Projects and POUs
  • Change logic in Program Organization Units (POUs).
  • Copy/paste POUs within or between sessions.
  • Rename or delete POUs whose variables are not referenced by
    Micro800
    controller configuration.
  • Reset initial values of UDFB instances.
  • Synchronize updates to references from UDFBs or UDFs.
  • Save or export projects.
  • Change the order of POUs in
    Project Organizer
    .
  • In the
    Parameter
    window, change parameters of UDFs or UDFBs that are not referenced by global variables.
  • Export programs.
  • Rename or delete POUs whose variables are referenced by
    Micro800
    controller configuration.
  • Add or delete interrupt POUs and change the properties of interrupts.
  • Remove or rename devices.
  • Import projects, POUs, or variables with the XLSX format.
  • Perform download or upload.
  • Change controller.
Tip:
  • Changing a defined word in RMC mode does not download the changes to the controller. To download the defined word changes to the controller, include additional changes along with the defined word change.
  • RMC changes that add comments to arrays or structures not referenced by the
    Micro800
    controller configuration cannot be downloaded to the controller.
  • After changing the project value of global or local variables in RMC mode, when reconnecting to the controller, you cannot enter RMC mode again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal