Variable parameters
The variable parameters displayed in the variable grid vary with:
Parameter | Description |
|---|---|
Name | The variable name Variable naming conventions are as follows:
The naming convention is based on the IEC-61131 rules for identifiers. |
Alias | A short name used in graphical language editors. An alias name contains no more than 128 ASCII characters. |
Data Type | The type of the variable Supported types are:
For information about data types, see Data types overview. |
Dimension | The size or the number of elements of an array For example, [1..3,1..10] represents a two-dimensional array containing a total of 30 elements. The recommended maximum size limit for a multi-dimensional array is [1..400,1..40]. |
Value | When the controller is offline, it shows the last known value of the variable in memory. When the controller is online, it shows the live value of the variable in memory. Values are not available with Micro810 LC10 controllers.It uses the syntax corresponding to the Data Type . |
Initial Value | The value of a variable when the controller starts execution for the first time. For example, after a program download. If the value is not retained, the initial value is the value of a variable after a controller power cycle. The initial value can be the default value or the value that is defined by the user when creating the variable. It uses the syntax corresponding to the Data Type . |
Comment | User-defined text A comment contains no more than 250 ASCII characters. |
String Size | The length of a string variable It is available for the string data type. The value is from 1 through 252. |
External Access | Determines whether to allow data exchange for the variable between the controller and FactoryTalk Design Workbench .Options are:
By default, most global variables can be accessed using symbolic addressing over a Common Industrial Protocol network, such as a human-machine interface using EtherNet/IP, unless access rights are defined in the variable grid. |
Direction | The role of a variable as an input variable, an output variable, or an internal variable Options are:
|
Attribute | The property of a variable that indicates its accessibility for reading and writing Options are:
|
Retained | It is available for user-defined variables. It determines the value to be restored to the variable after a power cycle.
The parameter is available for Micro810 LC10, Micro820 L20E, and Micro870 L70E controllers.
The variable values for other Micro800 controllers are retained
after a power cycle.By default, when creating a variable:
|
Provide Feedback