Automatic reference updates for global variables
When renaming a global variable in the
Micro800
project, the references to the global variable are automatically updated with the new variable name.Automatic name changes are reflected in references to global variables in:
- Ladder diagram Program Organization Units (POU)
- Function block diagram POUs
- Structured text POUs
- User-defined function blocks (UDFB) in POUs
- User-defined functions (UDF) in POUs
- Controller configurations
- Modbus mapping (Micro820L20E,Micro850L50E, andMicro870L70E controllers)
- MicroLogix mapping (Micro850L50E andMicro870L70E controllers)
- DNP3 mapping (2080-L70E-24QBBN and 2080-L70E-24QWBN controllers)
- Data log (Micro820L20E controllers)
- Recipe (Micro820L20E controllers)
After renaming a global variable:
- References to the variable are updated with the new name.
- For an unopened POU, UDFB, or UDF that is not password-protected, the associated editor automatically opens to show the variable name change.
- TheMicro800configuration page and theData protectiondialog do not open automatically. Manually open them to verify the name change.
- For a password-protected POU, UDFB, or UDF in the project, a message appears stating that not all variable references were updated with the new name.
Provide Feedback