Default system variables
The default system variables for
Micro800
controllers are available in the global variables grid.Variable Name | Type | Read/Write | Description |
|---|---|---|---|
__SYSVA_ABORT_CYCLE | BOOL | Read | Canceling cycle. |
__SYSVA_CCEXEC | BOOL | Read/Write | Execute one cycle when the application is in cycle-to-cycle mode. |
__SYSVA_CYCLECNT | DINT | Read | Cycle counter. |
__SYSVA_CYCLEDATE | TIME | Read | Time stamp of the beginning of the cycle in milliseconds. |
__SYSVA_FIRST_SCAN | BOOL | Read | First scan bit. True only on the first scan after that go to run. |
__SYSVA_KVBCERR | BOOL | Read/Write | Kernel variable binding consuming error or consumption error. |
__SYSA_KVBPERR | BOOL | Read | Kernel variable binding producing error or production error. |
__SYSVA_MAJ_ERR_HALT | BOOL | Read | Fault indicator. |
__SYSVA_POWERUP_BIT | BOOL | Read | Power up bit.
True only in the first scan after a power-up or running a new ladder for the first time. |
__SYSVA_PROJ_INCOMPLETE | UDINT | Read | Project incomplete.
BIT 0:
BIT 1:
|
__SYSVA_REMOTE | BOOL | Read | Indicates the switch position of the remote switch. |
__SYSVA_RESMODE | SINT | Read | Resource execution mode. Possible modes are:
-1: Fatal error. -2: Resource is stopped in stepping mode after exception. -3: Resource is stopped in stepping mode after division by zero exception. -4: Resource is stopped in stepping mode after bound check exception. -5: Maximum negative value for stepping. 1: Stored resource available. 2: Ready to run. 3: Run in real time. 4: Run in cycle by cycle. 5: Run with breakpoint encountered. 7: Stopped in stepping mode. 8: Micro800 programming mode.9: Micro800 suspend mode.10: Micro800 download mode - no program is loaded. |
__SYSVA_RESNAME | STRING | Read | System variable showing controller model name. For example, Micro810 LC10. (max length = 255). |
__SYSVA_SCANCNT | DINT | Read | Input scan counter. |
__SYSVA_SUSPEND_ID | UINT | Read | Suspend ID for SUS instruction block. |
_SYSVA_TCYCURRENT | TIME | Read | Current cycle time. Current cycle time and maximum cycle time fluctuate due to variabilities in the project such as user program and communications. |
__SYSVA_TCYCYCTIME | TIME | Read/Write | Programmed cycle time. Programmed cycle time is implemented in a resolution of 10 ms. If the entered value is not a multiple of 10, it will be rounded up to the next multiple of 10. |
__SYSVA_TCYMAXIMUM | TIME | Read | Maximum cycle time since last start. Current cycle time and maximum cycle time fluctuate due to variabilities in the project, such as user program and communications. |
__SYSVA_TCYOVERFLOW | DINT | Read | Number of cycle overflows. Micro810 LC10 system variable values cannot be retained during a
power down. To save system variable values, they must be copied to a retained user
variable. The value of _SYSVA_TCYOVERFLOW increases when (SYSVA_TCYCYCTIME)-(actual scan time) is smaller than or equals 10 ms. |
__SYSVA_TCYWDG | UDINT | Read/Write | Watchdog timeout. User Program watchdog timeout don't configured more than 2.55 seconds. |
__SYSVA_USER_DATA_LOST | BOOL | Read/Write | User data lost. True when Retentive User Data is cleared. Remains True until cleared by user or on a new User Program download. User Data Lost is TRUE when the controller powers up with certain Hard Faults and is only able to restore the User Program but not the Retentive User Data. |
Provide Feedback