Back up programs and project files to the memory module

Use the
Back up to the memory module
button on the 2080-MEMBAK-RTC2 plug-in module configuration page to back up user programs and controller project files to the 2080-MEMBAK-RTC2 plug-in module.
Prerequisites
  • The 2080-MEMBAK-RTC2 plug-in module is detected.
  • The controller is in
    Remote program
    mode.
To back up programs and project files to the memory module
  1. In
    Project Organizer
    , go to
    I/O Configurations
    Plug-in
    , and then do one of the following:
    • Double -click
      2080-MEMBAK-RTC2
      .
    • Select
      2080-MEMBAK-RTC2
      , and then select the
      Enter
      key.
  2. On the
    2080-MEMBAK-RTC2
    page, select
    Memory Module
    .
  3. On the
    Memory Module
    configuration page, select
    Back up to the memory module
    .
  4. In
    Memory module
    , select
    Back up
    .
  5. Select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal