Hardware and software requirements
In the example project, an
Micro870
L70E controller is used. You can use
an Micro820
L20E or Micro850
L50E controller
instead.The example project requires the following hardware and software components:
- FactoryTalk Design Workbench
- Ethernet driver, which is optional
- Micro870L70E controller (2080-L70E-24QBB)
- 24-volt DC power supply (2080-PS120-240VAC or equivalent)
- 2080-MEMBAK-RTC2 plug-in module
- 2080-IF4 plug-in module
Provide Feedback