Download the project to the controller
Use the steps to download the Traffic Light project to the
Micro870
L70E
controller, change the controller to Remote run
mode, and then verify
that the controller is running.To download the project to the controller
- Verify that the keyswitch on theMicro870L70E controller is in the center position (inRemote programmode).
- (optional) Build the project by doing one of the following:
- From the menu bar, select .
- Right-click the controller, and then selectBuild.
- Use theOutputpane to verify that building was successful. Fix any errors in the program before you download it.
- Download the project by doing one of the following:
- From the menu bar, select
. In Online center, select the checkbox beside the controller, and then selectDownload. - InProject Organizer, right-click the controller, and then selectDownload.
- Verify whether the Traffic Light project is running in the controller using the following steps:
- Verify that the run light on the controller is green without red lights.
- Open theConnectionpane, and then verify thatController modeisRunorRemote run.
Provide Feedback