Create a ladder diagram program

Use the steps to create a ladder diagram (LD) program, and then rename the program.
To create a ladder diagram
  1. In
    Project Organizer
    , right-click
    Programs
    , and then select
    New program
    .
  2. In
    New program
    , do the following:
    1. Enter the program name
      Traffic_Light_Control
      .
    2. From the
      Type
      list, select
      Ladder diagram
      .
  3. Select
    Create
    .
  4. Save the project by doing one of the following:
    • From the menu bar, select save button.
    • From the
      File
      menu, select
      Save
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal