FactoryTalk Design Workbench overview

FactoryTalk® Design Workbench™
is an on-premises development environment that provides web-based access for configuring devices and programming
Micro800™
controllers.
FactoryTalk Design Workbench
version 1.01.00 supports
Micro800
controllers, allowing one controller in each project. Later versions will support more devices.
Rockwell Automation
recognizes that some of the terms that are currently used in our industry and in this publication are not in alignment with the movement toward inclusive language in technology. We are proactively collaborating with industry peers to find alternatives to such terms and making changes to our products and content. Please excuse the use of such terms in our content while we implement these changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal