Export programs, function blocks, variables, and user-defined data types
Depending on the element type, the file formats for import and export are different.
- The following elements are exported to M8A files:
- Programs, including local variables and interrupts
- Function blocks, including local variables
- Functions, including local variables
- User-defined data types, including array data types, defined words, and structure data types
- Data logs
- Recipes
- The following elements are exported to CSV or XLSX files:
- Modbus mappings
- MicroLogix mappings
- DNP3 mappings
- Global and local variables
Provide Feedback