Register an ODBC Extractor
Perform the following steps to register an ODBC extractor:
- On the Management Console, select theExtractor Infotab.The Extractor list is displayed.Extractor Info Tab
- Click the Add [+] icon.TheExtractor Info Detailpage is displayed.Extractor Info Detail screen
- Provide a unique name for your Extractor. The Source Name works as the identifier for your extractor. You can search for an extractor with the Source Name. By default, DataMosaix generates a source name.Source Name example: EXT_1406230728_createproject_v1.Here, EXT stands for extractor, 140623 is the date in ddmmyy format, 0728 is the timestamp in hhmm format, and createproject_v1 is the project in which you are currently working. You can use the default source name or create your own.
- Provide the location details for which you are creating the extractor. This information can help you to identify an extractor when you have many extractors for different plants/sites/locations.
- From theAssociated Rolesdrop-down list, select at least one role. You can refer to various roles and capabilities by clickingRole Reference.You can select multiple roles from the Associated Roles drop-down list. In the search bar, you can search for any specific role from the list. If you want to apply all the roles to the application, select theSelect Allcheckbox.NOTE:The Associated Roles drop-down is visible and available only for Project Admin users or users within the Organization with a Project Admin Role assigned.Next, you can select a pipeline or create a new pipeline. When you create a new pipeline, you have the option of selecting from an existing dataset or creating a new dataset.
- From the pipeline drop-down, select a pipeline. On selecting a pipeline, the Pipeline External ID and Dataset Name fields are generated.To create a new pipeline, select the+ Create Pipelineoption.The Create Pipeline dialog box is displayed.
- Provide the following Pipeline information to create a new pipeline:
- Pipeline Name
- Pipeline External ID
- Pipeline Description
- When you create a pipeline, you can either select an existing dataset or create a new dataset. Select a Dataset from the drop-down if you want to use an existing Dataset.If you choose to create a new Dataset, the Dataset related fields are displayed. Provide the following dataset information:
- Dataset Name
- Dataset Description
- ClickAdd. Based on the options you choose (select or create), the Pipeline and Dataset information is either generated or created and displayed on the Extractor Info Detail page.
- Select the source type of extractor as ODBC.The fields relevant to the ODBC extractor appear on the screen for you to fill in details.Extractor Info Detail - ODBC Extractor
- In theTablefield, provide a table name. If this table does not exist, it will be created inside the database that is created in step 7.
- In thePrimary keyfield, provide a primary key for the table. For example, ID
- In theRaw databasefield, provide a database name. If this database does not exist, the database is created in the cdf project.
- In theQueryfield, enter a query to fetch records.
- In theConnection stringfield, enter the ODBC connection string to establish the connection.NOTE:TheSave and Applybutton enables after you provide all the required details.
- ClickSave and Apply.TheGenerated info Saveddialog box is displayed and it contains the configuration information. You can view the configuration file details by clickingView generated configuration file. Alternatively, you can also copy and save the information for future use by clicking Copy All. More importantly, you can download the .yml file that includes all the configuration information that you can use to run the extractor.Extractor Configuration File Download
- ClickDownload.The .yml file is downloaded in the Downloads folder of your local machine.
- ClickCloseto close the dialog box.The new extractor is displayed under Extractor Listing.
- Navigate to your project in CDF by clicking [Continue to Main Site] and selectIntegrate>Prepare data for transformation.Connect to Source Systems
- ClickCreate Database.
- ClickCreate table. Provide a unique name for the table. The table name cannot be changed later.
- SelectCreate empty tableand clickCreate.
- Download the extractor to your local machine.
- Copy the downloaded .yml file to the folder where the extractor is installed.
- Run the extractor on the command line.
- Once the extractor has been configured and executed successfully, navigate to your project in CDF and open the pipeline you created earlier.
- Click the pipeline link to verify the pipeline run details.
- SelectIntegrate>Prepare data for transformationto verify if the data is inserted into the table.
Provide Feedback