Supported Fields for the Assets Table

The following table provides the supported fields for the Assets table:
Supported Fields for the Assets Table
Column Name
Column Type
Description
Example
id
bigint
A server-generated ID for the object.
454501654069443
createdTime
timestamp
Timestamp when asset was created.
2019-09-07T15:50+00Z
lastUpdatedTime
timestamp
Timestamp when asset was updated.
2019-09-07T15:50+00Z
rootId
bigint
The ID of the root asset. The root asset is the asset spanning the entire asset hierarchy that this asset belongs to.
3039255880161656
name
varchar
The name of the asset.
function-variable-test
externalId
varchar
The external ID provided by the client. It must be unique for the resource type.
CDF_ExternalID
description
varchar
The description of the asset.
CDF project: testing_purpose
dataSetId
bigint
The id of the dataset this asset belongs to.
7166729101688251
source
varchar
The source of the asset.
test
parentExternalId
varchar
The external ID of the parent. The property will not be permitted if the asset does not have a parent or if the parent does not have externalId.
ftdm-parent-externalId
parentId
bigint
The ID of the parent of this node is null if it is the root node.
3281201682942258
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal