Prepare Tableau parameterized sheet
Perform the following steps to prepare Tableau parameterized sheet:
- ClickSheet1from the bottom-left corner.
- Drag and drop the following columns in theRowsfield:
- IdandNamecolumns underAssetstable.
- Id (Timeseries)column undertimeseriestable.
- timeseriesidandvaluenumericcolumns underCustom SQL Querytable.Drag and Drop Columns

- UnderParameters, selectShow Parameterfrom thesetParamTimesIddrop-down list.Click Show Parameter

- From the right pane, select any value from thesetParamTimesIddrop-down list.Select Value
All associated data will be displayed.Associated Data
Provide Feedback