Search
FactoryTalk DataMosaix SaaS Help
Supported Versions
The supported
Microsoft
Excel
version is 2412.
The supported PostgreSQL JDBC driver version is 9.1-901-1.jdbc4.
The supported Npgsql version is 4.0.17.
Configure Microsoft Excel to Connect to a Virtual PostgreSQL Data Interface
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal