Prerequisites
- MicrosoftExcelis installed.
- Access toFactoryTalk DataMosaix SaaSis available.
- The user has the Data Scientist role assigned within theFactoryTalk DataMosaix SaaSapplication. This role is required to create applications.
- The application is registered inFactoryTalk DataMosaix SaaSusing the Machine-to-Machine application type. For information on registering an application inFactoryTalk DataMosaix SaaS, refer to Register Application.
Provide Feedback