Prerequisites
- Power BI Desktop application is installed.
- Access toFactoryTalk DataMosaix SaaS.
- The Data Scientist role is assigned to create applications inFactoryTalk DataMosaix SaaS.
- Register the application using the Machine-to-Machine type inFactoryTalk DataMosaix SaaS. For information on registering an application inFactoryTalk DataMosaix SaaS, refer to Register Application.
Provide Feedback