Extractor and Application Methods
The following tables provide information on the extractors and applications methods that can be accessed by the users with associated roles.
Methods | Roles |
GET List of Extractors | APPLICATION DEVELOPER |
PROJECT ADMIN | |
DATA CONFIGURATOR | |
DATA SCIENTIST | |
APPLICATION USER | |
Delete Extractor | DATA CONFIGURATOR |
Register Extractor | DATA CONFIGURATOR |
Update Extractor | DATA CONFIGURATOR |
Methods | Roles |
GET List of Applications | APPLICATION DEVELOPER |
PROJECT ADMIN | |
DATA CONFIGURATOR | |
DATA SCIENTIST | |
APPLICATION USER | |
Delete Application | DATA SCIENTIST |
Register Application | DATA SCIENTIST |
Update Application | DATA SCIENTIST |
Provide Feedback